Solid Edge FrameworkSupport Type Library
Extend Method
Double that specifies the coordinates of the point at which the referenced element is to be extended.
Double that specifies the coordinates of the point at which the referenced element is to be extended.
The object to which the referenced element is to extend.
Description
Extends open graphic elements to a specified location.
Syntax
Visual Basic
Public Sub Extend( _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal TargetObj As Object _
) 
Parameters
x
Double that specifies the coordinates of the point at which the referenced element is to be extended.
y
Double that specifies the coordinates of the point at which the referenced element is to be extended.
TargetObj
The object to which the referenced element is to extend.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create an arc
    Set objArc1 = objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, _
                                              yStart:=0, xEnd:=0, yEnd:=0.05)
    ' Create a Line object
    Set objL1 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
                Lines2d.AddBy2Points(x1:=-0.05, y1:=-0.01, x2:=-0.05, y2:=0.05)
    ' Extend the Arc to the Line
    Call objArc1.Extend(x:=0, y:=0.05, TargetObj:=objL1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objArc1 = Nothing
    Set objL1 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members