Solid Edge FrameworkSupport Type Library
GetEndPoint Method
The coordinates of the endpoint for the referenced object.
The coordinates of the endpoint for the referenced object.
Description
Returns the coordinates of the end point of the referenced object.
Syntax
Visual Basic
Public Sub GetEndPoint( _
   ByRef x As Double, _
   ByRef y As Double _
) 
Parameters
x
The coordinates of the endpoint for the referenced object.
y
The coordinates of the endpoint for the referenced object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim x As Double
    Dim y As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create an arc
    Set objArc1 = objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, _
                                              yStart:=0, xEnd:=0, yEnd:=0.05)
    ' Get the EndPoint of the Arc
    Call objArc1.GetEndPoint(x:=x, y:=y)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objArc1 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members