Solid Edge FrameworkSupport Type Library
Index Property
Description
Returns the numeric index for the active object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Index As Long
Remarks
This index is the sequence that the object holds in its collection object (as held by the parent).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim lngIdx As Long
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create an arc
    Set objArc1 = objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, _
                                              yStart:=0, xEnd:=0, yEnd:=0.05)
    ' Get the Index Property of Arc object
    lngIdx = objArc1.Index
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objArc1 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members