Solid Edge FrameworkSupport Type Library
IsFillet Property
Description
Specifies whether or not the referenced Arc2d object is a fillet.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsFillet As Boolean
Remarks
If an Arc2d object is created with the AddAsFillet method, the arc may be a fillet. This means that it is an arc with fillet relationships to two other objects. The IsFillet property tests the Arc2d object to determine if it is a fillet. Use the Fillet property to access the FilletGeometry2d object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objL2 As SolidEdgeFrameworkSupport.Line2d
    Dim bIsFill As Boolean
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create two intersecting line objects
    Set objL1 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
                Lines2d.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    Set objL2 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
                Lines2d.AddBy2Points(x1:=0, y1:=0.1, x2:=0, y2:=0)
    ' Create an arc object
    Set objArc1 = objArcs.AddAsFillet(Obj1:=objL1, Obj2:=objL2, Radius:=0.05, _
                                      xDirection:=0.15, yDirection:=0.05)
    bIsFill = objArc1.IsFillet
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objL1 = Nothing
    Set objL2 = Nothing
    Set objArc1 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members