Solid Edge FrameworkSupport Type Library
Layer Property
Description
Sets and returns the named layer on which the referenced object resides.
Property type
Read-write property
Syntax
Visual Basic
Public Property Layer As String
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objArc2d As SolidEdgeFrameworkSupport.Arc2d
    Dim strlay As String
    Dim strlay1 As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create the arc2d object
    Set objArc2d = objSheet.Arcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                       xStart:=0.382, yStart:=0.105, xEnd:=0.2207, yEnd:=0.329)
    'get the layer of the object
    strlay = objArc2d.Layer
    'set a layer
    Call objSheet.Layers.Add("TopLayer")
    objArc2d.Layer = "TopLayer"
    'get the new layer
    strlay1 = objArc2d.Layer
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objArc2d = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members