Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
Dim objL1 As SolidEdgeFrameworkSupport.Line2d
Dim objL2 As SolidEdgeFrameworkSupport.Line2d
Dim objRelns As SolidEdgeFrameworkSupport.Relationships2d
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Create an Arcs collection object
Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
' Create two intersecting line objects
Set objL1 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
Lines2d.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
Set objL2 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
Lines2d.AddBy2Points(x1:=0, y1:=0.1, x2:=0, y2:=0)
' Create an arc object
Set objArc1 = objArcs.AddAsFillet(Obj1:=objL1, Obj2:=objL2, Radius:=0.05, _
xDirection:=0.15, yDirection:=0.05)
' Get the Relationships of Arc object
Set objRelns = objArc1.Relationships
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objArcs = Nothing
Set objL1 = Nothing
Set objL2 = Nothing
Set objArc1 = Nothing
End Sub