Solid Edge FrameworkSupport Type Library
RemoveAllSegmentedStyles Method
Description
Removes all segments defined for the referenced graphic object.
Syntax
Visual Basic
Public Sub RemoveAllSegmentedStyles() 
Remarks
Removing segmented styles does not remove the geometry. Instead, it removes the linear styles applied to the graphic object defined by the segments. If a segment is blank (for example, when the linear style is null), it reappears when its segment is removed.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objStyle1 As SolidEdgeFrameWork.LinearStyle
    Dim objStyle2 As SolidEdgeFrameWork.LinearStyle
    Dim objArcs2d As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc2d As SolidEdgeFrameworkSupport.Arc2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'get arcs2d object
    Set objArcs2d = objSheet.Arcs2d
    'create an arc2d
    Set objArc2d = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                 xStart:=0.15, yStart:=0#, xEnd:=0#, yEnd:=0.15)
    'get 2nos linear style object
    Set objStyle1 = objDoc.LinearStyles(3)
    Set objStyle2 = objDoc.LinearStyles(7)

    'Add first SegmentedStyle
    Call objArc2d.AddSegmentedStyle(x1:=0.15, y1:=0#, x2:=0.08116, _
                                    y2:=0.12615, Style:=objStyle1)
    'Add second SegmentedStyle
    Call objArc2d.AddSegmentedStyle(x1:=0.08116, y1:=0.12615, x2:=0.2, _
                                    y2:=0.3, Style:=objStyle2)
    'remove all segmented styles
    Call objArc2d.RemoveAllSegmentedStyles
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objArcs2d = Nothing
    Set objArc2d = Nothing
    Set objStyle1 = Nothing
    Set objStyle2 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members