Solid Edge FrameworkSupport Type Library
SegmentedStyleCount Property
Description
Returns the number of segmented styles defined for the referenced graphic object.
Property type
Read-only property
Syntax
Visual Basic
Public Property SegmentedStyleCount As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objStyle1 As SolidEdgeFrameWork.LinearStyle
    Dim objStyle2 As SolidEdgeFrameWork.LinearStyle
    Dim objStyle3 As SolidEdgeFrameWork.LinearStyle
    Dim objArcs2d As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc2d As SolidEdgeFrameworkSupport.Arc2d
    Dim LngStyCnt As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create arcs2d object
    Set objArcs2d = objSheet.Arcs2d
    'create an arc2d
    Set objArc2d = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                 xStart:=0.15, yStart:=0#, xEnd:=0, yEnd:=-0.15)
    'get 3nos linear style object
    Set objStyle1 = objDoc.LinearStyles(3)
    Set objStyle2 = objDoc.LinearStyles(7)
    Set objStyle3 = objDoc.LinearStyles(5)
    'AddSegmentedStyle 1
    Call objArc2d.AddSegmentedStyle(x1:=0.15, y1:=0#, x2:=0#, y2:=0.15, _
                                    Style:=objStyle1)
    'AddSegmentedStyle 2
    Call objArc2d.AddSegmentedStyle(x1:=0#, y1:=0.15, x2:=-0.15, y2:=0#, _
                                    Style:=objStyle2)
    'AddSegmentedStyle 3
    Call objArc2d.AddSegmentedStyle(x1:=-0.15, y1:=0#, x2:=0, y2:=-0.15, _
                                    Style:=objStyle3)
    'get segmented style count
    LngStyCnt = objArc2d.SegmentedStyleCount
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objArcs2d = Nothing
    Set objArc2d = Nothing
    Set objStyle1 = Nothing
    Set objStyle2 = Nothing
    Set objStyle3 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members