Solid Edge FrameworkSupport Type Library
SendBackward Method
Description
Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display but when you do not want to send the object all the way to the back of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objArcs2d As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc2d1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objArc2d2 As SolidEdgeFrameworkSupport.Arc2d
    Dim objArc2d3 As SolidEdgeFrameworkSupport.Arc2d
    Dim Lngorder1 As Long
    Dim Lngorder2 As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' create arcs2d object
    Set objArcs2d = objSheet.Arcs2d
    'create arc2d objects
    Set objArc2d1 = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                  xStart:=0.15, yStart:=0#, xEnd:=0, yEnd:=0.15)
    Set objArc2d2 = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                  xStart:=0#, yStart:=0.15, xEnd:=-0.15, yEnd:=0#)
    Set objArc2d3 = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                  xStart:=0#, yStart:=0.15, xEnd:=-0.15, yEnd:=0#)
    'get Zorder of objArc2d3 before sending backward
    Lngorder1 = objArc2d3.ZOrder
    'send the third arc2d backward
    Call objArc2d3.SendBackward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objArcs2d = Nothing
    Set objArc2d1 = Nothing
    Set objArc2d2 = Nothing
    Set objArc2d3 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members