Solid Edge FrameworkSupport Type Library
SendToBack Method
Description
Changes the display order of visible objects by moving the referenced object behind all overlapping objects.
Syntax
Visual Basic
Public Sub SendToBack() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display. The SendBackward method can also be used.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objArcs2d As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc2d1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objArc2d2 As SolidEdgeFrameworkSupport.Arc2d
    Dim objArc2d3 As SolidEdgeFrameworkSupport.Arc2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' create arcs2d object
    Set objArcs2d = objSheet.Arcs2d
    'create arc2d objects
    Set objArc2d1 = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                  xStart:=0.15, yStart:=0#, xEnd:=0, yEnd:=0.15)
    Set objArc2d2 = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                  xStart:=0#, yStart:=0.15, xEnd:=-0.15, yEnd:=0#)
    Set objArc2d3 = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                  xStart:=0#, yStart:=0.15, xEnd:=-0.15, yEnd:=0#)
    'send the third arc2d to back
    Call objArc2d3.SendToBack
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objArcs2d = Nothing
    Set objArc2d1 = Nothing
    Set objArc2d2 = Nothing
    Set objArc2d3 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members