Solid Edge FrameworkSupport Type Library
SetMajorAxis Method
Specifies the x value of the major axis vector.
Specifies the y value of the major axis vector.
Description
Sets the x and y values of the major axis vector for the referenced object.
Syntax
Visual Basic
Public Sub SetMajorAxis( _
   ByVal x As Double, _
   ByVal y As Double _
) 
Parameters
x
Specifies the x value of the major axis vector.
y
Specifies the y value of the major axis vector.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim x As Double, y As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create an arc
    Set objArc1 = objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, _
                                              yStart:=0, xEnd:=0, yEnd:=0.05)
    ' Reset the MajorAxis
    Call objArc1.SetMajorAxis(x:=0.1, y:=0)
    ' Get the MajorAxis coordinates of the Arc
    Call objArc1.GetMajorAxis(x:=x, y:=y)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objArc1 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members