Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-only property
Syntax
Visual Basic
Public Property Style As GeometryStyle2d
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objArcs2d As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc2d As SolidEdgeFrameworkSupport.Arc2d
    Dim objSty As SolidEdgeFrameworkSupport.GeometryStyle2d
    Dim strdashna As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' create arcs2d object
    Set objArcs2d = objSheet.Arcs2d
    'create an arc2d
    Set objArc2d = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                 xStart:=0.15, yStart:=0#, xEnd:=0, yEnd:=0.15)
    'get style of arc2d
    Set objSty = objArc2d.Style
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objArcs2d = Nothing
    Set objArc2d = Nothing
    Set objSty = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members