Solid Edge FrameworkSupport Type Library
Trim Method
Specifies the x value of the direction point in which the trim is to take place.
Specifies the y value of the direction point in which the trim is to take place.
Specifies the first object that intersects this object. The intersection point of the object determines the trim point.
Specifies the second object that intersects this object. This intersection point of the object determines the second trim point.
Description
Deletes sections of geometry that intersect other objects.
Syntax
Visual Basic
Public Sub Trim( _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal CutObj1 As Object, _
   Optional ByVal CutObj2 As Variant _
) 
Parameters
x
Specifies the x value of the direction point in which the trim is to take place.
y
Specifies the y value of the direction point in which the trim is to take place.
CutObj1
Specifies the first object that intersects this object. The intersection point of the object determines the trim point.
CutObj2
Specifies the second object that intersects this object. This intersection point of the object determines the second trim point.
Remarks
If one object is specified, it is trimmed from the intersection point of the objects in the direction of the point specified. If two objects are specified, the trim is in the section of the object specified by the direction point. For example, if the direction point is between the two input objects, the section of this object to be trimmed is between the points the two objects intersect this object. If the direction point is outside of the two input objects, the trim is from the intersection of the object closest to the direction point, in the opposite direction of the other input object intersection point. The resulting objects are put into the select set. In some cases, a single object can be trimmed and two objects are the result.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objL2 As SolidEdgeFrameworkSupport.Line2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    Dim x As Double, y As Double
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create an arc
    Set objArc1 = objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, _
                                              yStart:=0, xEnd:=-0.05, yEnd:=0)
    ' Create a Line object which intersects the Arc object
    Set objL1 = objDoc.ProfileSets(1).Profiles(1). _
                Lines2d.AddBy2Points(x1:=0, y1:=-0.1, x2:=0, y2:=0.1)

    ' Trim the Arc
    Call objArc1.Trim(x:=-0.05, y:=0, CutObj1:=objL1)
    ' Get the End Point
    Call objArc1.GetEndPoint(x:=x, y:=y)
    If Abs(x - 0) > 0.00001 Or y <> 0.05 Then
        MsgBox ("Error in the Trim method of Arc object")
    End If

    ' Delete all the Objects
    Call objArc1.Delete
    Call objL1.Delete
    ' Create an arc
    Set objArc1 = objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0, _
                                              yStart:=-0.05, xEnd:=-0.05, yEnd:=0)
    ' Create 2 Line objects which intersects the Arc object
    Set objL1 = objDoc.ProfileSets(1).Profiles(1).Lines2d. _
                AddBy2Points(x1:=-0.1, y1:=0, x2:=0.1, y2:=0)
    Set objL2 = objDoc.ProfileSets(1).Profiles(1).Lines2d. _
                AddBy2Points(x1:=0, y1:=-0.01, x2:=0, y2:=0.1)
    ' Trim the Arc
    Call objArc1.Trim(x:=0.05, y:=0, CutObj1:=objL1, CutObj2:=objL2)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objArc1 = Nothing
    Set objL1 = Nothing
    Set objL2 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members