Solid Edge FrameworkSupport Type Library
AddSegmentedStyle Method
Double that specify the coordinates for the start of the segment.
Double that specify the coordinates for the start of the segment.
Double that specify the coordinates for the end of the segment.
Double that specify the coordinates for the end of the segment.
Specifies the LinearStyle2d object to assign to the segment.
Description
Defines a segment on a graphic object and assigns a linear style to that segment.
Syntax
Visual Basic
Public Sub AddSegmentedStyle( _
   ByVal x1 As Double, _
   ByVal y1 As Double, _
   ByVal x2 As Double, _
   ByVal y2 As Double, _
   ByVal Style As Object _
) 
Parameters
x1
Double that specify the coordinates for the start of the segment.
y1
Double that specify the coordinates for the start of the segment.
x2
Double that specify the coordinates for the end of the segment.
y2
Double that specify the coordinates for the end of the segment.
Style
Specifies the LinearStyle2d object to assign to the segment.
Remarks
To define the segment, this method accepts two points that specify the start and end of the segment. If a linear style does not exist for the formatting required for the segment, create the linear style through the LinearStyles collection object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objBSpln1 As SolidEdgeFrameworkSupport.BSplineCurve2d
    Dim objLinStyle As SolidEdgeFrameWork.LinearStyle
    Dim MyArray(9) As Double
    Dim strStyleName As String, strStyleParent As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Define an Array of Points
    MyArray(0) = 0.05
    MyArray(1) = 0.05
    MyArray(2) = 0.09
    MyArray(3) = 0.12
    MyArray(4) = 0.14
    MyArray(5) = 0.05
    MyArray(6) = 0.19
    MyArray(7) = 0.18
    MyArray(8) = 0.25
    MyArray(9) = 0.09
    'Create a BSplineCurve object
    Set objBSpln1 = objSheet.BSplineCurves2d.AddByPoints(Order:=4, ArraySize:=5, _
                                                         Array:=MyArray())
    ' Create a LinearStyle2d Object
    strStyleName = "LinearStyleDotted"
    strStyleParent = "Dotted"
    Set objLinStyle = objDoc.LinearStyles.Add(Name:=strStyleName, _
                                              Parent:=strStyleParent)
    ' Add a SegmentedStyle to the BSplineCurve
    Call objBSpln1.AddSegmentedStyle(x1:=0.14, y1:=0.05, x2:=0.25, _
                                     y2:=0.09, Style:=objLinStyle)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objBSpln1 = Nothing
    Set objLinStyle = Nothing
End Sub
See Also

BSplineCurve2d Object  | BSplineCurve2d Members