Solid Edge FrameworkSupport Type Library
Evaluate Method
Specifies the parameter you want to evaluate.
Specifies the point of the location specified by Parameter.
Specifies the first derivative of the location specified by Parameter.
Specifies the second derivative of the location specified by Parameter.
Specifies the curvature of the location specified by Parameter.
Description
This method takes the input parameter location and returns the point, first derivative, second derivative, and curvature of the location for the referenced BSplineCurve2d object.
Syntax
Visual Basic
Public Sub Evaluate( _
   ByVal Parameter As Double, _
   Optional ByRef Point As Variant, _
   Optional ByRef FirstDerivative As Variant, _
   Optional ByRef SecondDerivative As Variant, _
   Optional ByRef Curvature As Variant _
) 
Parameters
Parameter
Specifies the parameter you want to evaluate.
Point
Specifies the point of the location specified by Parameter.
FirstDerivative
Specifies the first derivative of the location specified by Parameter.
SecondDerivative
Specifies the second derivative of the location specified by Parameter.
Curvature
Specifies the curvature of the location specified by Parameter.
See Also

BSplineCurve2d Object  | BSplineCurve2d Members