Solid Edge FrameworkSupport Type Library
Extend Method
Double that specifies the coordinates of the point at which the referenced element is to be extended.
Double that specifies the coordinates of the point at which the referenced element is to be extended.
The object to which the referenced element is to extend.
Description
Extends open graphic elements to a specified location.
Syntax
Visual Basic
Public Sub Extend( _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal TargetObj As Object _
) 
Parameters
x
Double that specifies the coordinates of the point at which the referenced element is to be extended.
y
Double that specifies the coordinates of the point at which the referenced element is to be extended.
TargetObj
The object to which the referenced element is to extend.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBSplns As SolidEdgeFrameworkSupport.BSplineCurves2d
    Dim objBSpln1 As SolidEdgeFrameworkSupport.BSplineCurve2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim MyArray(9) As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Define an Array of Points
    MyArray(0) = 0
    MyArray(1) = 0
    MyArray(2) = 0.03
    MyArray(3) = 0.02
    MyArray(4) = 0.04
    MyArray(5) = 0.01
    MyArray(6) = 0.05
    MyArray(7) = 0.08
    MyArray(8) = 0.07
    MyArray(9) = 0.04
    'Create a BSplineCurves collection object
    Set objBSplns = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                        objDoc.RefPlanes(1)).BSplineCurves2d

    'Create a BSplineCurve object
    Set objBSpln1 = objBSplns.AddByPoints(Order:=4, ArraySize:=5, Array:=MyArray())
    If objBSpln1.NodeCount <> 5 Then
        MsgBox ("Error in the Extend method")
    End If
    ' Create a Line object
    Set objLine1 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                       objDoc.RefPlanes(1)).Lines2d.AddBy2Points _
                                                       (x1:=0.06, y1:=0.035, x2:=0.09, y2:=0.035)
    ' Extend the object
    Call objBSpln1.Extend(x:=0.09, y:=0.1, TargetObj:=objLine1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBSplns = Nothing
    Set objBSpln1 = Nothing
    Set objLine1 = Nothing
End Sub
See Also

BSplineCurve2d Object  | BSplineCurve2d Members