Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objBSpln1 As SolidEdgeFrameworkSupport.BSplineCurve2d
Dim objLinStyle1 As SolidEdgeFrameWork.LinearStyle
Dim objLinStyle2 As SolidEdgeFrameWork.LinearStyle
Dim MyArray(9) As Double
Dim strStyleName As String, strStyleParent As String
Dim dblX1 As Double, dblY1 As Double, dblX2 As Double, dblY2 As Double
Dim objStyle As Object
Dim lngIdx As Long
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
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Define an Array of Points
MyArray(0) = 0.05
MyArray(1) = 0.05
MyArray(2) = 0.09
MyArray(3) = 0.12
MyArray(4) = 0.14
MyArray(5) = 0.05
MyArray(6) = 0.19
MyArray(7) = 0.18
MyArray(8) = 0.25
MyArray(9) = 0.09
'Create a BSplineCurve object
Set objBSpln1 = objSheet.BSplineCurves2d.AddByPoints(Order:=4, ArraySize:=5, _
Array:=MyArray())
' Create a LinearStyle2d Object
strStyleName = "LinearStyleDotted"
strStyleParent = "Dotted"
Set objLinStyle1 = objDoc.LinearStyles.Add(Name:=strStyleName, _
Parent:=strStyleParent)
' Add a SegmentedStyle to the BSplineCurve
Call objBSpln1.AddSegmentedStyle(x1:=0.05, y1:=0.05, x2:=0.14, _
y2:=0.05, Style:=objLinStyle1)
' Create a LinearStyle2d Object
strStyleName = "LinearStyleDashed"
strStyleParent = "Center"
Set objLinStyle2 = objDoc.LinearStyles.Add(Name:=strStyleName, _
Parent:=strStyleParent)
' Add a SegmentedStyle to the BSplineCurve
Call objBSpln1.AddSegmentedStyle(x1:=0.14, y1:=0.05, x2:=0.19, _
y2:=0.18, Style:=objLinStyle2)
' Add 3rd SegmentedStyle to the BSplineCurve
Call objBSpln1.AddSegmentedStyle(x1:=0.19, y1:=0.18, x2:=0.25, _
y2:=0.09, Style:=objLinStyle1)
' Get the SegmentedStyle
Call objBSpln1.GetSegmentedStyle(Index:=2, x1:=dblX1, y1:=dblY1, _
x2:=dblX2, y2:=dblY2, Style:=objStyle)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objBSpln1 = Nothing
Set objLinStyle1 = Nothing
Set objLinStyle2 = Nothing
End Sub