Solid Edge FrameworkSupport Type Library
Range Method
Specifies the x coordinate of the lower-left corner the referenced object.
Specifies the y coordinate of the lower-left corner of the referenced object.
Specifies the x coordinate of the upper-right corner of the referenced object.
Specifies the y coordinate of the upper-right corner of the referenced object.
Description
Returns the high and low range values for the referenced object.
Syntax
Visual Basic
Public Sub Range( _
   ByRef XMinimum As Double, _
   ByRef YMinimum As Double, _
   ByRef XMaximum As Double, _
   ByRef YMaximum As Double _
) 
Parameters
XMinimum
Specifies the x coordinate of the lower-left corner the referenced object.
YMinimum
Specifies the y coordinate of the lower-left corner of the referenced object.
XMaximum
Specifies the x coordinate of the upper-right corner of the referenced object.
YMaximum
Specifies the y coordinate of the upper-right corner of the referenced object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBSplns As SolidEdgeFrameworkSupport.BSplineCurves2d
    Dim objBSpln1 As SolidEdgeFrameworkSupport.BSplineCurve2d
    Dim MyArray(9) As Double
    Dim vRng As Variant
    Dim x1 As Double, y1 As Double, x2 As Double, y2 As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Define an Array of Points
    MyArray(0) = 0
    MyArray(1) = 0
    MyArray(2) = 0.03
    MyArray(3) = 0.02
    MyArray(4) = 0.04
    MyArray(5) = 0.01
    MyArray(6) = 0.05
    MyArray(7) = 0.08
    MyArray(8) = 0.07
    MyArray(9) = 0.04
    'Create a BSplineCurves collection object
    Set objBSplns = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                        objDoc.RefPlanes(1)).BSplineCurves2d

    'Create a BSplineCurve object
    Set objBSpln1 = objBSplns.AddByPoints(Order:=4, ArraySize:=5, Array:=MyArray())
    ' Get the Range of the Curve
    vRng = objBSpln1.Range(xMinimum:=x1, yMinimum:=y1, xMaximum:=x2, yMaximum:=y2)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBSplns = Nothing
    Set objBSpln1 = Nothing
End Sub
See Also

BSplineCurve2d Object  | BSplineCurve2d Members