Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-only property
Syntax
Visual Basic
Public Property Style As GeometryStyle2d
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objBSpln1 As SolidEdgeFrameworkSupport.BSplineCurve2d
    Dim objLinStyle As SolidEdgeFrameWork.LinearStyle
    Dim objBSplnStyle As SolidEdgeFrameworkSupport.GeometryStyle2d
    Dim MyArray(9) As Double
    Dim strStyleName As String, strStyleParent As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Define an Array of Points
    MyArray(0) = 0.05
    MyArray(1) = 0.05
    MyArray(2) = 0.09
    MyArray(3) = 0.12
    MyArray(4) = 0.14
    MyArray(5) = 0.05
    MyArray(6) = 0.19
    MyArray(7) = 0.18
    MyArray(8) = 0.25
    MyArray(9) = 0.09
    'Create a BSplineCurve object
    Set objBSpln1 = objSheet.BSplineCurves2d.AddByPoints(Order:=4, ArraySize:=5, _
                                                         Array:=MyArray())
    ' Create a LinearStyle2d Object
    strStyleName = "LinearStyleDotted"
    strStyleParent = "Dotted"
    Set objLinStyle = objDoc.LinearStyles.Add(Name:=strStyleName, Parent:=strStyleParent)

    ' Add a SegmentedStyle to the BSplineCurve
    Call objBSpln1.AddSegmentedStyle(x1:=0.14, y1:=0.05, x2:=0.25, _
                                     y2:=0.09, Style:=objLinStyle)
    ' Get the Style property
    Set objBSplnStyle = objBSpln1.Style
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objBSpln1 = Nothing
    Set objLinStyle = Nothing
    Set objBSplnStyle = Nothing
End Sub
See Also

BSplineCurve2d Object  | BSplineCurve2d Members