Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objCircle As SolidEdgeFrameworkSupport.Circle2d
Dim objBalloons As SolidEdgeFrameworkSupport.Balloons
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' getting the Balloons collection object on the active sheet
Set objBalloons = objSheet.Balloons
' drawing a circle on the sheet
Set objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.05)
' adding two balloons on the active sheet
Call objBalloons.AddByTerminator(TerminatorObject:=objCircle, x1:=0.75, y1:=0.05, z1:=0, keyPoint1:=True)
Call objBalloons.AddByTerminator(TerminatorObject:=objCircle, x1:=0.75, y1:=0.015, z1:=0, keyPoint1:=False)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objCircle = Nothing
Set objBalloons = Nothing
End Sub