Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objBalloons As SolidEdgeFrameworkSupport.Balloons
Dim lngCount As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' getting the Balloons collection object on the active sheet
Set objBalloons = objSheet.Balloons
' adding a balloon on the active sheet
Call objBalloons.Add(x1:=0.25, y1:=0.25, z1:=0)
' getting the count of the Balloons on the sheet
lngCount = objBalloons.Count
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objBalloons = Nothing
End Sub