Solid Edge FrameworkSupport Type Library
IsAcceptableConnectElementOrMember Property
Description
This read-only Boolean property returns True if the object specified is on the same sheet as the referenced BoltHoleCircle object.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsAcceptableConnectElementOrMember( _
   ByVal Object As Object _
) As Boolean
Parameters
Object
See Also

BoltHoleCircle Collection  | BoltHoleCircle Members