Solid Edge FrameworkSupport Type Library
DashName Property
Description
Sets and returns the named dash style for the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property DashName As String
Remarks
The name that you assign to this property must be the name of an existing dash style. For Solid fill types, the get and set properties are not applicable. For Hatch fill types, the property returns the name of the dash style if all hatch lines have the same dash style. Setting the property overrides the dash style of all hatch lines in the fill.
See Also

BoundaryStyle2d Object  | BoundaryStyle2d Members