Solid Edge FrameworkSupport Type Library
FillType Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
BoundaryStyle2d Object
: FillType Property
Description
Sets and returns the type of the fill style that is associated with the referenced Boundary2d object.
Property type
Read-only property
Syntax
Visual Basic
Public Property FillType As Long
Remarks
The type indicates if it is a solid fill or a hatch fill.
See Also
BoundaryStyle2d Object
|
BoundaryStyle2d Members