Solid Edge FrameworkSupport Type Library
Scale Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
BoundaryStyle2d Object
: Scale Property
Description
Sets or returns the scale for the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Scale As Double
Remarks
Legal values for the scale factor include only positive numbers. (The scale factor must be non-negative and non-zero.)
See Also
BoundaryStyle2d Object
|
BoundaryStyle2d Members