Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-write property
Syntax
Visual Basic
Public Property Style As DimensionStyle
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines
    Dim objCLStyle As SolidEdgeFrameworkSupport.DimensionStyle
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' getting the CenterLines collection object on the active sheet
    Set objCenterLines = objDoc.ActiveSheet.CenterLines
    ' setting the dimension style of the CenterLines collection object to 'ANSI'
    objCenterLines.Style = objDoc.DimensionStyles(1)
    ' getting the style object of the CenterLines collection object
    Set objCLStyle = objCenterLines.Style
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCenterLines = Nothing
    Set objCLStyle = Nothing
End Sub
See Also

CenterLines Collection  | CenterLines Members