Solid Edge FrameworkSupport Type Library
GetEndPoint Method
The coordinates of the endpoint for the referenced object.
The coordinates of the endpoint for the referenced object.
The coordinates of the endpoint for the referenced object.
Description
Returns the coordinates of the end point of the referenced object.
Syntax
Visual Basic
Public Sub GetEndPoint( _
   ByRef x As Double, _
   ByRef y As Double, _
   ByRef z As Double _
) 
Parameters
x
The coordinates of the endpoint for the referenced object.
y
The coordinates of the endpoint for the referenced object.
z
The coordinates of the endpoint for the referenced object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines
    Dim objCenterLine As SolidEdgeFrameworkSupport.CenterLine
    Dim dblX As Double, dblY As Double, dblZ As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the CenterLines object on the active sheet
    Set objCenterLines = objSheet.CenterLines

    ' Draw a CenterLine on the active sheet
    Set objCenterLine = objCenterLines.Add(x1:=0.25, y1:=0.15, z1:=0, _
                                           x2:=0.25, y2:=0.35, z2:=0)
    ' Get the EndPoint
    Call objCenterLine.GetEndPoint(x:=dblX, y:=dblY, z:=dblZ)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterLines = Nothing
    Set objCenterLine = Nothing
End Sub
See Also

CenterLine Object  | CenterLine Members