Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
    Dim objCMApp As SolidEdgeFramework.Application
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' getting the active sheet
    Set objSheet = objDoc.ActiveSheet
    ' getting the CenterMarks collection object on the active sheet
    Set objCenterMarks = objSheet.CenterMarks
    ' getting the application object of the CenterMarks collection object
    Set objCMApp = objCenterMarks.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterMarks = Nothing
    Set objCMApp = Nothing
End Sub
See Also

CenterMarks Collection  | CenterMarks Members