Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
Dim lngCount As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' getting the active sheet
Set objSheet = objDoc.ActiveSheet
' getting the CenterMarks collection object on the active sheet
Set objCenterMarks = objSheet.CenterMarks
' adding a center mark on the active sheet
Call objCenterMarks.Add(x:=0.25, y:=0.25, z:=0)
' getting the count in the CenterMarks collection object
lngCount = objCenterMarks.Count
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objCenterMarks = Nothing
End Sub