Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-write property
Syntax
Visual Basic
Public Property Style As DimensionStyle
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
    Dim objCMStyle As SolidEdgeFrameworkSupport.DimensionStyle
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' getting the active sheet
    Set objSheet = objDoc.ActiveSheet
    ' getting the CenterMarks collection object on the active sheet
    Set objCenterMarks = objSheet.CenterMarks
    ' setting the Style of the CenterMarks collection object
    objCenterMarks.Style = objDoc.DimensionStyles(1)
    ' getting the Style object of the CenterMarks collection object
    Set objCMStyle = objCenterMarks.Style
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterMarks = Nothing
    Set objCMStyle = Nothing
End Sub
See Also

CenterMarks Collection  | CenterMarks Members