Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
Dim objCenterMark As SolidEdgeFrameworkSupport.CenterMark
Dim objLine As SolidEdgeFrameworkSupport.Line2d
Dim objCirc As SolidEdgeFrameworkSupport.Circle2d
Dim lngZorder1 As Long, lngZorder2 As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' Get the CenterMarks collection object on the active sheet
Set objCenterMarks = objSheet.CenterMarks
' Create a CenterMark on the active sheet
Set objCenterMark = objCenterMarks.Add(x:=0.25, y:=0.25, z:=0)
' Get the Zorder
lngZorder1 = objCenterMark.ZOrder
' Create a line objcet
Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.2, y1:=0.25, x2:=0.4, y2:=0.25)
' Create a circle object
Set objCirc = objSheet.Circles2d.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.06)
' Apply BringForward method to CenterMark object
Call objCenterMark.BringForward
' Get the Zorder
lngZorder2 = objCenterMark.ZOrder
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objCenterMarks = Nothing
Set objCenterMark = Nothing
Set objLine = Nothing
Set objCirc = Nothing
End Sub