Solid Edge FrameworkSupport Type Library
Index Property
Description
Returns the numeric index for the active object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Index As Long
Remarks
This index is the sequence that the object holds in its collection object (as held by the parent).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
    Dim objCenterMark1 As SolidEdgeFrameworkSupport.CenterMark
    Dim objCenterMark2 As SolidEdgeFrameworkSupport.CenterMark
    Dim lngIdx As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the CenterMarks collection object on the active sheet
    Set objCenterMarks = objSheet.CenterMarks
    ' Create CenterMarks on the active sheet
    Set objCenterMark1 = objCenterMarks.Add(x:=0.25, y:=0.25, z:=0)
    Set objCenterMark2 = objCenterMarks.Add(x:=0.35, y:=0.25, z:=0)
    ' Get the Index
    lngIdx = objCenterMark2.Index

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterMarks = Nothing
    Set objCenterMark1 = Nothing
    Set objCenterMark2 = Nothing
End Sub
See Also

CenterMark Object  | CenterMark Members