Solid Edge FrameworkSupport Type Library
SendBackward Method
Description
Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display but when you do not want to send the object all the way to the back of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
    Dim objCenterMark As SolidEdgeFrameworkSupport.CenterMark
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objCirc As SolidEdgeFrameworkSupport.Circle2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Create a line objcet
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
    ' Create a circle object
    Set objCirc = objSheet.Circles2d.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.06)
    ' Get the CenterMarks collection object on the active sheet
    Set objCenterMarks = objSheet.CenterMarks
    ' Create a CenterMark on the active sheet
    Set objCenterMark = objCenterMarks.Add(x:=0.25, y:=0.25, z:=0)
    ' Apply SendBackward method to CenterMark object
    Call objCenterMark.SendBackward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterMarks = Nothing
    Set objCenterMark = Nothing
    Set objLine = Nothing
    Set objCirc = Nothing
End Sub
See Also

CenterMark Object  | CenterMark Members