Solid Edge FrameworkSupport Type Library
Type Property
Description
Specifies the type of the object being referenced.
Property type
Read-only property
Syntax
Visual Basic
Public Property Type As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
    Dim objCenterMark As SolidEdgeFrameworkSupport.CenterMark
    Dim lngType As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the CenterMarks collection object on the active sheet
    Set objCenterMarks = objSheet.CenterMarks
    ' Create a CenterMark on the active sheet
    Set objCenterMark = objCenterMarks.Add(x:=0.25, y:=0.25, z:=0)
    ' Get the Type
    lngType = objCenterMark.Type

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterMarks = Nothing
    Set objCenterMark = Nothing
End Sub
See Also

CenterMark Object  | CenterMark Members