Solid Edge FrameworkSupport Type Library
GetConnectedObjects Method
Returns the first object to which the chamfer or fillet connects.
Returns the second object to which the chamfer or fillet connects.
Description
Returns both objects connected to the referenced fillet or chamfer.
Syntax
Visual Basic
Public Sub GetConnectedObjects( _
   ByRef Obj1 As Object, _
   ByRef Obj2 As Object _
) 
Parameters
Obj1
Returns the first object to which the chamfer or fillet connects.
Obj2
Returns the second object to which the chamfer or fillet connects.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine3 As SolidEdgeFrameworkSupport.Line2d
    Dim objChamferGeom2d As SolidEdgeFrameworkSupport.ChamferGeometry2d
    Dim objConnObj1 As SolidEdgeFrameworkSupport.Line2d
    Dim objConnObj2 As SolidEdgeFrameworkSupport.Line2d
    Dim dblAng As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Lines2d
    ' Create 2 Line2d objects
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    Set objLine2 = objLines.AddBy2Points(x1:=0.1, y1:=0, x2:=0.1, y2:=0.1)
    ' Create another Line object using the AddAsChamfer Method
    Set objLine3 = objLines.AddAsChamfer(Obj1:=objLine1, Obj2:=objLine2, xDirection:=0.2, _
                                         yDirection:=0.2, SetBackA:=0.04, SetBackB:=0.04)
    Set objChamferGeom2d = objLine3.Chamfer
    ' Get the ConnectedObjects
    'Named arguments will be implemented after fixing the TR#38344
    'Call objChamferGeom2d.GetConnectedObjects(objConnObj1, objConnObj2)
    '10/21/98 - Bobba : The named arguments problem couldn't be found on 06.00.00.18.
    'Hence changing the code to test with Named arguments.
    Call objChamferGeom2d.GetConnectedObjects(Obj1:=objConnObj1, Obj2:=objConnObj2)
    'TR#38541 logged for reverse retreval of connected objects
    'TR#38541 was set as WAD.
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
    Set objLine3 = Nothing
    Set objChamferGeom2d = Nothing
    Set objConnObj1 = Nothing
    Set objConnObj2 = Nothing
End Sub
See Also

ChamferGeometry2d Object  | ChamferGeometry2d Members