Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
Dim objLine3 As SolidEdgeFrameworkSupport.Line2d
Dim objChamferGeom2d As SolidEdgeFrameworkSupport.ChamferGeometry2d
Dim dblAng As Double
Dim dblSetBackA As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create an empty Lines2d collection object
Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Lines2d
' Create 2 Line2d objects
Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
Set objLine2 = objLines.AddBy2Points(x1:=0.1, y1:=0, x2:=0.1, y2:=0.1)
' Create another Line object using the AddAsChamfer Method
Set objLine3 = objLines.AddAsChamfer(Obj1:=objLine1, Obj2:=objLine2, xDirection:=0.05, _
yDirection:=0.03, SetBackA:=0.04, SetBackB:=0.04)
Set objChamferGeom2d = objLine3.Chamfer
' Get the SetBackA of the Chamfer
dblSetBackA = objChamferGeom2d.SetBackA
objChamferGeom2d.SetBackA = 0.01
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objLines = Nothing
Set objLine1 = Nothing
Set objLine2 = Nothing
Set objLine3 = Nothing
Set objChamferGeom2d = Nothing
End Sub