Solid Edge FrameworkSupport Type Library
BringToFront Method
Description
Changes the display order of the referenced object by moving it in front of all other overlapping objects.
Syntax
Visual Basic
Public Sub BringToFront() 
Remarks
This command is useful when objects are hidden by other objects that are filled and have a higher priority display. The BringForward method can also be used.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objCirc2 As SolidEdgeFrameworkSupport.Circle2d
    Dim objCirc3 As SolidEdgeFrameworkSupport.Circle2d
    Dim lngZorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the Circles collection object
    Set objCircs = objSheet.Circles2d
    ' Ceate circle objects
    Set objCirc1 = objCircs.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.06)
    Set objCirc2 = objCircs.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.07)
    Set objCirc3 = objCircs.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.08)
    'Get the Zorder of Cirlce1
    lngZorder = objCirc1.ZOrder
    ' Apply BringToFront method
    objCirc1.BringToFront
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCircs = Nothing
    Set objCirc1 = Nothing
    Set objCirc2 = Nothing
    Set objCirc3 = Nothing
End Sub
See Also

Circle2d Object  | Circle2d Members