Solid Edge FrameworkSupport Type Library
Circumference Property
Description
Returns the dimension along the line of a circle or ellipse.
Property type
Read-only property
Syntax
Visual Basic
Public Property Circumference As Double
Remarks
The circumference value is always around the complete object for objects that are partially trimmed or hidden.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim dblCircum As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a Circles collection object
    Set objCircs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Circles2d
    ' Create a Circle object
    Set objCirc1 = objCircs.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
    ' Get the Circumference of the Circle object
    dblCircum = objCirc1.Circumference
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCircs = Nothing
    Set objCirc1 = Nothing
End Sub
See Also

Circle2d Object  | Circle2d Members