Solid Edge FrameworkSupport Type Library
IsAttributeSetPresent Property
Description
Returns True if a specified Attribute Set exists on the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsAttributeSetPresent( _
   ByVal Name As String _
) As Boolean
Parameters
Name
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objAttributeSets As Object
    Dim bAttribSetPresent As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' Create a Circles collection object
    Set objCircs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Circles2d
    ' Create a Circle object
    Set objCirc1 = objCircs.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
    ' Get the AttributeSets collection object
    Set objAttributeSets = objCirc1.AttributeSets
    'Create an AttributeSet
    Call objAttributeSets.Add("MyAttribSet")
    'Check for the presence of created Attributeset
    bAttribSetPresent = objCirc1.IsAttributeSetPresent("MyAttribSet")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCircs = Nothing
    Set objCirc1 = Nothing
    Set objAttributeSets = Nothing
End Sub
See Also

Circle2d Object  | Circle2d Members