Solid Edge FrameworkSupport Type Library
Scale Method
Specifies the factor by which the referenced object is to be scaled.
Description
Scales the referenced object by a specified factor.
Syntax
Visual Basic
Public Sub Scale( _
   ByVal Factor As Double _
) 
Parameters
Factor
Specifies the factor by which the referenced object is to be scaled.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objCirc2 As SolidEdgeFrameworkSupport.Circle2d
    Dim vTemp As Variant
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the Circles collection object
    Set objCircs = objSheet.Circles2d
    ' Ceate a circle object
    Set objCirc1 = objCircs.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.06)
    ' Enlarge the circle object by scale method
    vTemp = objCirc1.Scale(Factor:=2)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCircs = Nothing
    Set objCirc1 = Nothing
    Set objCirc2 = Nothing
End Sub
See Also

Circle2d Object  | Circle2d Members