Solid Edge FrameworkSupport Type Library
SetCenterPoint Method
Specifies the x coordinate for the new center point.
Specifies the y coordinate of the new center point.
Description
Relocates the center point of the specified object.
Syntax
Visual Basic
Public Sub SetCenterPoint( _
   ByVal x As Double, _
   ByVal y As Double _
) 
Parameters
x
Specifies the x coordinate for the new center point.
y
Specifies the y coordinate of the new center point.
Remarks
The new center point is specified in x and y coordinates. As a result of the SetCenterPoint method, the object is repositioned with respect to the new center point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim x As Double, y As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a Circles collection object
    Set objCircs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Circles2d
    ' Create a Circle object
    Set objCirc1 = objCircs.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
    ' Reset the CenterPoint of the Circle
    Call objCirc1.SetCenterPoint(x:=0.05, y:=0.05)
    ' Get the CenterPoint of the Circle
    Call objCirc1.GetCenterPoint(x:=x, y:=y)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCircs = Nothing
    Set objCirc1 = Nothing
End Sub
See Also

Circle2d Object  | Circle2d Members