Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-only property
Syntax
Visual Basic
Public Property Style As GeometryStyle2d
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objStyle As SolidEdgeFrameworkSupport.GeometryStyle2d
    Dim strVisible As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the Circles collection object
    Set objCircs = objSheet.Circles2d
    ' Create a circle object
    Set objCirc1 = objCircs.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.06)
    ' Get the circle object style
    Set objStyle = objCirc1.Style
    ' Get the Linear name property of circle object
    strVisible = objStyle.LinearName
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCircs = Nothing
    Set objCirc1 = Nothing
    Set objStyle = Nothing
End Sub
See Also

Circle2d Object  | Circle2d Members