Solid Edge FrameworkSupport Type Library
AddByCenterRadius Method
Specifies the x coordinate of the center of the circle.
Specifies the y coordinate of the center of the circle.
Specifies the radius of the circle.
Description
Uses a center point and radius to create a Circle2d object.
Syntax
Visual Basic
Public Function AddByCenterRadius( _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal Radius As Double _
) As Circle2d
Parameters
x
Specifies the x coordinate of the center of the circle.
y
Specifies the y coordinate of the center of the circle.
Radius
Specifies the radius of the circle.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a Circles collection object
    Set objCircs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Circles2d
    ' Create a Circle object
    Call objCircs.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCircs = Nothing
End Sub
See Also

Circles2d Collection  | Circles2d Members