Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objCircPats2d As SolidEdgeFrameworkSupport.CircularPatterns2d
    Dim objCircPat As SolidEdgeFrameworkSupport.CircularPattern2d
    Dim objCircPatApp As SolidEdgeFramework.Application
    Dim lngCount As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get hold of CircularPatterns2d object
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(prefplanedisp:=objDoc.RefPlanes(1))
    Set objCircPats2d = objProfile.CircularPatterns2d

    'Create a CircularPattern2d with AddCircle method with offsettype as sePatternFillOffset
    Set objCircPat = objCircPats2d.AddByCircle(CenterX:=0#, CenterY:=0#, StartX:=0.025, StartY:=0#, _
                                               Orientation:=igGeom2dOrientCounterClockwise, OffsetType:=sePatternFillOffset, Count:=5, _
                                               AngularSpacing:=20 * PI / 180)
    'Get the App object from CircularPatter2d object
    Set objCircPatApp = objCircPat.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objCircPats2d = Nothing
    Set objCircPat = Nothing
    Set objCircPatApp = Nothing
End Sub
See Also

CircularPattern2d Object  | CircularPattern2d Members