Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfile As SolidEdgePart.Profile
Dim objCircPats2d As SolidEdgeFrameworkSupport.CircularPatterns2d
Dim objCircPat As SolidEdgeFrameworkSupport.CircularPattern2d
Dim lngCount As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get hold of CircularPatterns2d object
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(prefplanedisp:=objDoc.RefPlanes(1))
Set objCircPats2d = objProfile.CircularPatterns2d
'Create a CircularPattern2d with AddCircle method with offsettype as sePatternFillOffset
Set objCircPat = objCircPats2d.AddByCircle(CenterX:=0#, CenterY:=0#, StartX:=0.025, StartY:=0#, _
Orientation:=igGeom2dOrientCounterClockwise, OffsetType:=sePatternFitOffset, Count:=5, _
AngularSpacing:=20 * PI / 180)
'Get the number of occurrences in the Pattern
lngCount = objCircPat.Count
'Set the number of occurrences in the Pattern
objCircPat.Count = 10
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfile = Nothing
Set objCircPats2d = Nothing
Set objCircPat = Nothing
End Sub