Solid Edge FrameworkSupport Type Library : CircularPatterns2d Collection |
![]() | Uses an arc definition (center point, start point, and sweep) to create a CircularPattern2d object. |
![]() | Creates a CircularPattern2d object by specifying a center point and point on the circle at which the pattern is to begin. |
![]() | The items in a collection. |
![]() | Returns the active application object. |
![]() | Returns the number of objects in the referenced collection. |
![]() | Returns the parent object for the referenced object. |