Solid Edge FrameworkSupport Type Library
BringToFront Method
Description
Changes the display order of the referenced object by moving it in front of all other overlapping objects.
Syntax
Visual Basic
Public Sub BringToFront() 
Remarks
This command is useful when objects are hidden by other objects that are filled and have a higher priority display. The BringForward method can also be used.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCompStrns As SolidEdgeFrameworkSupport.ComplexStrings2d
    Dim objCompStrn1 As SolidEdgeFrameworkSupport.ComplexString2d
    Dim objCompStrn2 As SolidEdgeFrameworkSupport.ComplexString2d
    Dim objCompStrn3 As SolidEdgeFrameworkSupport.ComplexString2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objL2 As SolidEdgeFrameworkSupport.Line2d
    Dim objL3 As SolidEdgeFrameworkSupport.Line2d
    Dim objL4 As SolidEdgeFrameworkSupport.Line2d
    Dim objL5 As SolidEdgeFrameworkSupport.Line2d
    Dim objL6 As SolidEdgeFrameworkSupport.Line2d
    Dim objBObjs1(0 To 1) As Object
    Dim objBObjs2(0 To 1) As Object
    Dim objBObjs3(0 To 1) As Object
    Dim lngZorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create ComplexStrings2d collection object
    Set objCompStrns = objSheet.ComplexStrings2d
    'Draw few lines on the active sheet
    Set objL1 = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.2)
    Set objL2 = objSheet.Lines2d.AddBy2Points(x1:=0.2, y1:=0.2, x2:=0.4, y2:=0.2)
    Set objL3 = objSheet.Lines2d.AddBy2Points(x1:=0.15, y1:=0.1, x2:=0.25, y2:=0.25)
    Set objL4 = objSheet.Lines2d.AddBy2Points(x1:=0.25, y1:=0.25, x2:=0.5, y2:=0.1)
    Set objL5 = objSheet.Lines2d.AddBy2Points(x1:=0.175, y1:=0.1, x2:=0.325, y2:=0.2)
    Set objL6 = objSheet.Lines2d.AddBy2Points(x1:=0.325, y1:=0.2, x2:=0.525, y2:=0.15)
    'Store the Objects in an Array
    Set objBObjs1(0) = objL1
    Set objBObjs1(1) = objL2
    Set objBObjs2(0) = objL3
    Set objBObjs2(1) = objL4
    Set objBObjs3(0) = objL5
    Set objBObjs3(1) = objL6
    'Create the ComplexString2d objects
    Set objCompStrn1 = objCompStrns.AddByObjects(ArraySize:=2, Members:=objBObjs1())
    Set objCompStrn2 = objCompStrns.AddByObjects(ArraySize:=2, Members:=objBObjs2())
    Set objCompStrn3 = objCompStrns.AddByObjects(ArraySize:=2, Members:=objBObjs3())
    'Get the ZOrder of the first ComplexString2d
    lngZorder = objCompStrn1.ZOrder
    'Bring the objCompStrn1 to front
    Call objCompStrn1.BringToFront

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCompStrns = Nothing
    Set objCompStrn1 = Nothing
    Set objCompStrn2 = Nothing
    Set objCompStrn3 = Nothing
    Set objL1 = Nothing
    Set objL2 = Nothing
    Set objL3 = Nothing
    Set objL4 = Nothing
    Set objL5 = Nothing
    Set objL6 = Nothing
    Set objBObjs1(0) = Nothing
    Set objBObjs1(1) = Nothing
    Set objBObjs2(0) = Nothing
    Set objBObjs2(1) = Nothing
    Set objBObjs3(0) = Nothing
    Set objBObjs3(1) = Nothing
End Sub
See Also

ComplexString2d Object  | ComplexString2d Members