Solid Edge FrameworkSupport Type Library
IsAttributeSetPresent Property
Description
Returns True if a specified Attribute Set exists on the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsAttributeSetPresent( _
   ByVal Name As String _
) As Boolean
Parameters
Name
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCompStrns As SolidEdgeFrameworkSupport.ComplexStrings2d
    Dim objCompStrn1 As SolidEdgeFrameworkSupport.ComplexString2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objL2 As SolidEdgeFrameworkSupport.Line2d
    Dim objL3 As SolidEdgeFrameworkSupport.Line2d
    Dim objBObjs(0 To 2) As Object
    Dim objAttributeSet As Object
    Dim bAttribPresent As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create ComplexStrings2d collection object
    Set objCompStrns = objSheet.ComplexStrings2d
    'Draw few lines on the active sheet
    Set objL1 = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.2)
    Set objL2 = objSheet.Lines2d.AddBy2Points(x1:=0.2, y1:=0.2, x2:=0.4, y2:=0.2)
    Set objL3 = objSheet.Lines2d.AddBy2Points(x1:=0.4, y1:=0.2, x2:=0.5, y2:=0.1)
    'Store the Objects in an Array
    Set objBObjs(0) = objL1
    Set objBObjs(1) = objL2
    Set objBObjs(2) = objL3
    'Create the ComplexString2d
    Set objCompStrn1 = objCompStrns.AddByObjects(ArraySize:=3, Members:=objBObjs())
    'Create an AttributeSet with Add method
    Set objAttributeSet = objCompStrn1.AttributeSets.Add("MyAttrib Set")
    'Get the boolean value of IsAttributeSetPresent
    bAttribPresent = objCompStrn1.IsAttributeSetPresent(Name:="MyAttrib Set")

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCompStrns = Nothing
    Set objCompStrn1 = Nothing
    Set objL1 = Nothing
    Set objL2 = Nothing
    Set objL3 = Nothing
    Set objBObjs(0) = Nothing
    Set objBObjs(1) = Nothing
    Set objBObjs(2) = Nothing
    Set objAttributeSet = Nothing
End Sub
See Also

ComplexString2d Object  | ComplexString2d Members