Solid Edge FrameworkSupport Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCompStrn As SolidEdgeFrameworkSupport.ComplexStrings2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objL2 As SolidEdgeFrameworkSupport.Line2d
    Dim objL3 As SolidEdgeFrameworkSupport.Line2d
    Dim objBObjs(1 To 3) As Object
    Dim lngCnt As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' getting the ComplexStrings2d object on the active sheet
    Set objCompStrn = objSheet.ComplexStrings2d
    'Draw few lines on the active sheet
    Set objL1 = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.2)
    Set objL2 = objSheet.Lines2d.AddBy2Points(x1:=0.2, y1:=0.2, x2:=0.4, y2:=0.2)
    Set objL3 = objSheet.Lines2d.AddBy2Points(x1:=0.4, y1:=0.2, x2:=0.5, y2:=0.1)
    ' Store the Objects in an Array
    Set objBObjs(1) = objL1
    Set objBObjs(2) = objL2
    Set objBObjs(3) = objL3
    ' Create a ComplexString2d object
    Call objCompStrn.AddByObjects(ArraySize:=3, Members:=objBObjs())
    ' Get the Count of the ComplexStrings2d on the active sheet
    lngCnt = objCompStrn.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCompStrn = Nothing
    Set objL1 = Nothing
    Set objL2 = Nothing
    Set objL3 = Nothing
    Set objBObjs(1) = Nothing
    Set objBObjs(2) = Nothing
    Set objBObjs(3) = Nothing
End Sub
See Also

ComplexStrings2d Collection  | ComplexStrings2d Members