Solid Edge FrameworkSupport Type Library
Parent Property
Description
Returns the parent object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Parent As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objCompStrn As SolidEdgeFrameworkSupport.ComplexStrings2d
    Dim objParent As SolidEdgeDraft.Sheet
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' getting the ComplexStrings2d object on the active sheet
    Set objCompStrn = objDoc.ActiveSheet.ComplexStrings2d
    ' getting the Parent object of the ComplexStrings2d collection object
    Set objParent = objCompStrn.Parent
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCompStrn = Nothing
    Set objParent = Nothing
End Sub
See Also

ComplexStrings2d Collection  | ComplexStrings2d Members